Technical FAQs

Ask a Question

What are the BMXNOC0402 ETH_STS indicator states?

If the ETH_STS is off this indicates that the module is not getting power.
A yellow ETH_STS on solid means that all tests passed and the module is healthy.
A yellow ETH_STS flashing 4 times indicates a duplicate IP address.
A yellow ETH_STS flashing 6 times indicates that the module is using its default IP address. 
 
Was this helpful?
What can we do to improve the information ?