Technical FAQs

Ask a Question

What is the pin assignment of the Lexium 28 CN1 solder type connector?

The attached image file shows the pin assignment of the solder terminals as viewed from the solder side of the 50 pin CN1 connector

 
Was this helpful?
What can we do to improve the information ?