Title
Unity 13 Hot Fix regarding BMENOP0300 module
Issue
Unity 13 Hot Fix regarding BMENOP0300 module
Product Line
M580 BMENOP0300
Environment
Unity Pro 13
Cause
N/A
Resolution What is new with UnityPro_V130_HF_BMENOP0300 Improvements
Description of issue or behavior (before installation of UnityPro_V130_HF_BMENOP0300 Improvements)
· On M580, the user can’t declare more than one BMENOP0300 module with the IP Forwarding configuration.
· with a M580 HSBY the user can't to validate the configuration with the address xx.xx.0.xx
New behavior after installation of UnityPro_V130_HF_BMENOP0300 Improvements
- On M580, user can declare more than one BMENOP0300 module with the IP Forwarding configuration.
Note: limitation is unchanged with BMENOC0321. This Hot Fix is only related to BMENOP0300
- With a HSBY cpu the user can validate the configuration with the address xx.xx.0.xx
What to do after installation of UnityPro_V130_HF_BMENOP0300 Improvements
A build of project is required
Compatibility - No compatibility break:
· Project done before Hot Fix installation can be open and built after hotfix installation.
· Project done after Hot Fix installation can be open and built before hotfix installation
·
Note : IP forwarding improvement is only supported with BMENOP0300 Firmware version V2.0