Technical FAQs

Ask a Question

Unity Backup Clear with a Quantum 140CPU43412

Title
Unity Backup Clear with a Quantum 140CPU43412
 
Issue
Unity Backup Clear with a Quantum 140CPU43412
 
Product Line
Quantum 140CPU43412
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 Connect to the CPU43412 with Unity 13.Then erase the Backup copy of the program by selecting Backup Clear in the Unity >> PLC >> Project Backup Menu.
The next time a download to the CU is executed, the new project will be backed up. Do a Project Backup compare to verify.
 
Was this helpful?
What can we do to improve the information ?