Technical FAQs

Ask a Question

How can I display the local time when %MW49...53 seem to be in UTC?

The system words %SW49...53 are in universal coordinated time (UTC), not in local time. If you require local time, use the RRTC_DT function block. (NOTE: RRTC_DT_MS is also in UTC time.) 
Was this helpful?
What can we do to improve the information ?