Technical FAQs

Ask a Question

Is there any provision for finger safe protection in 9422 disconnect switches of Square D

Yes, an additional barrier that helps prevent accidental contact with live parts. Fieldinstalled transparent barriers do not restrict visual inspection of the switch. Barriers provide IEC529 IP2X “finger safe” protection when door of enclosed disconnect switch is open. A convenient door allows use of test probes without accessing fuses and replacement of fuses without removing barrier. Barrier must be used with the skirt kit to enclose a panel mounted 9422 disconnect.

Please find attached document for selection of reference numbers.
Was this helpful?
What can we do to improve the information ?