Technical FAQs

Ask a Question

How to get into the broken mode of HMISTO735?

During the boot switch off the power twice after the boot bar reached 50% (or a bit more, maybe 75%). This will enable the broken mode, then the it can be easily download via USB stick or Ethernet to the target. 
Was this helpful?
What can we do to improve the information ?