Technical FAQs

Ask a Question

Why drive's version contains XX after the letter E in SoMove on Altivar Procress Drive?

 Issue:
Why drive's version contains XX after the letter E in SoMove on Altivar Procress Drive?

Product Line:
Altivar ATV630, ATV930

Environment:
All model numbers, all serial numbers.

Cause:
Customer wanted to verify the firmware version of the drive with the firmware version in SoMove file.

Resolution:
It's normal to have XX on device version and communication channel/options.  It's SoMove limitation.
User-added image

 
Was this helpful?
What can we do to improve the information ?