Browse FAQs

Can I configure the VW3A1101 keypad for split screen display when using it with an ATV212 series drive or S-flex enclosed system?

Published date: 17 December 2018

Issue:
Customer wants to display multiple parameters simultaneously on the VW3A1101 graphic keypad when connected to an ATV212 series drive or SFD series S-flex.

Product line:
ATV212 open style and enclosed S-flex systems.

Environment:
All models, All serial numbers.

Cause:
Unable to find instructions in manual.

Resolution:
This is not possible with the ATV212 series drives and S-flex systems.  The ATV212 drive is not capable of split screen display.  There are multiple monitoring parameters to choose from but only one can be displayed at any given time.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.