Technical FAQs

Ask a Question

TCSEFEA23F3F20 LED Flashes five times

Title
TCSEFEA23F3F20 LED Flashes five times
 
Issue
TCSEFEA23F3F20 LED Flashes five times
 
Product Line
TCSEFEA23F3F20  Connexium Firewall
 
Environment
Connexium
 
Cause
N/A
 
Resolution
 Per the user manual, The meaning of 5 flashes During a Load Sequence - The device was unable to load the files.
It is possible that the files were damaged during the copying operation. Erase the existing files and reload the configuration files from the configuration utility again.

 
Was this helpful?
What can we do to improve the information ?