Browse FAQs

M580 Ethernet RIO topology

Published date: 28 March 2019

Title
M580 Ethernet RIO topology
 
Issue
M580 Ethernet RIO topology
 
Product Line
M580
 
Environment
EcoStruxure Control Expert
 
Cause
N/A
 
Resolution
 When creating a Modicon M580 Ethernet RIO network the Daisy-Chain (Ring) architecture is absolutely necessary for the M580 ERIO system to perform properly.
The Star topography is not an approved architecture.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.