Technical FAQs

Ask a Question

ATV58 control board pinout 10 pins vs 9 pins?  What is the difference? 

Issue:
ATV58 control board pinout 10 pins vs 9 pins?  What is the difference? 

Product Line:
ATV58 

Environment:
All serial numbers 

Cause:
Not sure which pins to use. 

Resolution:
10 pin terminal has an additional AO1 terminal  located on the left side (not used) . Use the 9 pins on the right side of the terminal strip. 
Was this helpful?
What can we do to improve the information ?