Browse FAQs

Does Quantum Ethernet port support NTP

Published date: 28 March 2019

Title
Quantum Ethernet port and NTP
 
Issue
Quantum Ethernet port and NTP
 
Product Line
Quantum
 
Environment
EcoStruxure Control Expert
 
Cause
N/A
 
Resolution
 The NTP service is not available on the Quantum CPU Ethernet port.
You will need to use a 140NOE77111 module or a 140NOC78000 module that supports the NTP service.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.