Browse FAQs

BMXNOR0200H Response Time

Published date: 28 March 2019


Title
BMXNOR0200H Response using DirectNoAck
 
Issue
BMXNOR0200H Response Time
 
Product Line
BMXNOR0200
 
Environment
Unity
 
Cause
N/A
 
Resolution
 Changing the DNP3 point operate mode under DNP3 Net Client - Session 0 - Data Mapping from Direct to DirectNoAck will allows for a quicker response. 
The setting DirectNoAck does not confirm the point before using.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.