Technical FAQs

Ask a Question

Can Rapsody versions be installed in windows 10 operating system?

Schneider Electric recommends Windows 7 & 8 operating systems for the installation of Rapsody. 
Rapsody presently doesn't officially support windows 10, it may sometimes be possible to install but with certain limitations & we cannot guarantee the performance as with the supported operating systems.
To get an optimum working environment, we suggest & validated the installation of Rapsody in Windows 7 & 8.
Was this helpful?
What can we do to improve the information ?