Browse FAQs

Cannot enable Hotline tag (work tag) on the ADVC 2 controller

Published date: 28 May 2019

Issue   
Why does the newer ADVC 2 controllers not let one enable a hotline tag (work tag) in closed position.

Product Line   
ADVC 2

Resolution
Work Tag implementation has changed a bit since A45-37.00 to enhance more security to the user in this mode. In general the rules are:
- Work Tag can only be changed in suitable mode (Local Control or Remote Mode)
- Additional rules include:
+ Work Tag can NOT be applied when switchgear in CLOSED position and Protection is Off 
+ Work Tag can NOT be applied in both Open and CLosed position when battery is LOW



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.