Browse FAQs

M580 and Ethernet RemoteIO switches

Published date: 28 March 2019

Title
M580 and Ethernet RemoteIO switches
 
Issue
M580 and Ethernet RemoteIO switches
 
Product Line
M580 BMxCRA312x0 Connexium
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
The M580 connectivity to a RemoteIO Drop module is a proprietary solution.
That means you have to use only Schneider Ethernet RemoteIO capable switches for which Schneider supplies the correct configuration file.
Unfortunately, we do not have a solution involving the use of third party switches , such as Cisco.
Please review Chapter 2, in the  Modicon M580 - System Planning Guide for Complex Topologies, on the approved switches for use in a M580 Ethernet RemoteIO system.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.