Technical FAQs

Ask a Question

BCPM Communication Recommendation

Issue
Customer is asking if we would recommended RS-485 2-wire or RS-485 4-wire communication wiring?

Product Line
BCPM (Branch Circuit Power Meter)

Resolution
It is recommended to user either 2-wire or 4-wire RS-485 communication depending on the devices and what they can support. If your using a daisy-chain of devices with your BCPM, take a look at what those devices support and the determine which wiring (2-wire or 4-wire) the BCPM will use.
Was this helpful?
What can we do to improve the information ?