Technical FAQs

Ask a Question

Unity Pro: Is there a length limitation on a DTM Device name?

Yes, the name of the DTM Device is limited to 32 characters.
If the name exceeds 32 characters, the error produced on building the project is "Invalid  DTM name".
Was this helpful?
What can we do to improve the information ?