Browse FAQs

M580 and BMENOC03x1 Health bits

Published date: 27 March 2019

Title
M580 and BMENOC03x1 Health bits
 
Issue
M580 and BMENOC03x1 Health bits
 
Product Line
M580 PAC BMENOC03x1
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
With the M580, there is no separate DDT variable for HEALTH_BITS_IN array created.
The M580 and the NOC create a Device DDT with the Healthbits embedded within, for example, BMENOC0301_2.DIO_HEALTH[x] is used instead.
The bit identification for the health bits is as following,  BMENOC0301_2.DIO_HEALTH[0] for Device [000] in its Device List, BMENOC0301_2.DIO_HEALTH[1] for Device [001] in its Device List.

In addition, When you add a device via the DTM Browser a Device DDT will get created for that device based on the supplied name and that Device DDT will have Freshness bits, Inputs and Outputs sub elements in it.
The Freshness bits can also be used for monitoring connection Health.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.