Technical FAQs

Ask a Question

Can 140NOE771xx FTP access be disabled in a ProWORX/Unity application?

There is no solution for disabling the 140NOE771xx FTP when using Hardware that is programmed using anything other than Unity.
All Quantum controllers will have the FTP port opened when programmed with Concept/ProWORX. There is no way to disable it. All Unity Quantum CPU's running a copro version lower than v5.0 and all NOE's running firmware lower than v6.0 will have the FTP port opened. You must be running a CPU copro v5.0 or higher and NOE firmware v6.0 and higher in a Unity system before you have the option of disabling the FTP port. With the current firmware and Unity Software will have the option to disable the FTP in your Ethernet network configuration.
Was this helpful?
What can we do to improve the information ?