Technical FAQs

Ask a Question

What is the max frequency of the TM171/172 fast counter input ?

The maximum frequency for the TM171/TM172 fast counter input is 2 Khz.
Was this helpful?
What can we do to improve the information ?