Technical FAQs

Ask a Question

How to enter password to access parameter on VSD07 Drive?

 Issue:
How to enter password to access parameter on VSD07 Drive?

Product Line:
VSD07

Environment:
All serial numbers.

Cause:
Customer wanted to change speed reference of the drive.

Resolution:
To access the parameters, enter the program mode by pressing the Mode button.  This activates the Password prompt.  The display reads "00" and the right hand decimal point blinks.  Next, enter the four digit password.  Since the display is only two digits, this required two steps.  Press arrow up to scroll to the first 2 digits of password value.  Default password is 1225.  Press Mode to enter first two digits "12". 
Once the Mode button is pressed, the display changes to "00" and the right hand decimal point blinks more rapidly.  This indicates that the last two digits of the password must now be entered.  Right decimal point blinks faster.  Press arrow up to scroll to last 2 digits password value.  Press Mode to enter two digits "25".  When the Mode button is pressed, the right hand decimal point stays on instead of blinking, and "01" is displayed.  This indicates that the Program mode is accessed at the beginning of the parameter menu (01 is the first parameter.)
Was this helpful?
What can we do to improve the information ?