Browse FAQs

What is the default password for VSD07 drive?

Published date: 28 July 2019

Issue:
How can VSD07 be unlocked when it is password protected?

Product Line:
VSD07

Environment:
All serial numbers

Cause:
Customer needed to access to parameters to change the speed of the drive.

Resolution:
The default password of the drive is 1225.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.