Technical FAQs

Ask a Question

What is the purpose of Relay in PM1130H meter ?

Relay is used to trigger an alarm or a secondary system based on a preset condition in the meter.

The relay is Normally Open (NO) when not triggered. When triggered (operated) it changes to Normally Closed (NC).

A relay can be triggered depending on source of operation. The supplied source can be utility, alternate source, or both.
Was this helpful?
What can we do to improve the information ?