Technical FAQs

Ask a Question

SoMove Software, following TeSys firmware update, no longer sees the expansion module?

Issue:
SoMove Software, following TeSys firmware update, no longer sees the expansion module?

Product Line:
ATV

Environment:
All

Cause:
Wiring

Resolution:
After an LTMR update is complete and you cycle power, if there is an Alarm MS and a red status LED on the LTME option module that is the reason SoMove doesn't see it. There is an RJ45 Link between the 2 modules.  Disconnect the link and reconnect it, should see LED go from Red to Green. 
** Note:  This can most likely be avoided by disconnecting SoMove prior to the power cycle once the update completes.
Was this helpful?
What can we do to improve the information ?