Technical FAQs

Ask a Question

What is the inrush duration for the 140CPS11420 Power Supply?

After 1/4 cycle it is 95% charged up and after 1/2 cycle it is ready to go with no more inrush. If you need a time duration use 10ms for the specification.
Was this helpful?
What can we do to improve the information ?