Browse FAQs

What are the FDR parameters set to in the LTMCUF by default?

Published date: 28 November 2018

Issue:
Customer needs to know what the default configuration is for the FDR parameters in the LTMCUF HMI

Product Line:
Tesys T 

Environment:
LTMCUF only.  Does not apply to LTMCU

Cause:
NA

Resolution:
By default, when LTMCUF is new, the error F09 "No config valid" appears as the LTMCUF memory is empty. This is a reminder that a backup operation needs to be done before using the FDR services.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.