Technical FAQs

Ask a Question

How can you set up the ATV66 drive with VW3A66305 modbus plus card to have a HOA control?

Issue:
How can you set up the ATV66 drive with modbus plus to have a HOA control?

Product Line:
ATV66 with modbus plus module VW3A66305 . 

Environment:
All 

Cause:
Wants to set up a HOA for Hand is terminal control and auto is modbus plus control. 

Resolution:
Preferred wiring for the HOA would be example Force to Local is LI4  programming menu 7.2 (Force Local)
(Hand and OFF) will turn on LI4  terminal control 
(Auto) will turn off LI4  network control.

Ref 1 = AI1 speed pot for hand control speed ref 


 
Was this helpful?
What can we do to improve the information ?