Technical FAQs

Ask a Question

How can you set the Altivar Process Drive language back to English if someone accidentally changed it??

Issue:
How can I set my Altivar Process ATV630 or ATV930 back to English?

Product Line:
ATV600 ATV900 Altivar Process

Environment:
All

Cause:
Programming

Resolution:
If locked, Press Home + ESC to access the Home Screen
Press OK to Main Menu 
Scroll down to menu 8 > Press OK
Press OK again > You'll now see the list language options, 1st is English
Press OK on English, or desired language
Press the HOME button.
Was this helpful?
What can we do to improve the information ?