Technical FAQs

Ask a Question

M221 IO Scanning - Reset

When communications are lost during IO Scanning the communications need to be reset. %S112 for Modbus TCP and %S110 for Modbus Serial IOScanner. You can also add a bit reset in the Configuration.
Was this helpful?
What can we do to improve the information ?