Technical FAQs

Ask a Question

Can I use a GV2 on a Altivar drive output?

Issue: 
Can I use a GV2 on a Altivar drive output?    

Product Line:
Alitvar Drives

Environment: 
ATV61, ATV212, ATV71, ATV630, ATV930, ATV32, ATV320, ATV312, ATV12, ATV660, ATV340  

Cause
Application has 2 motors on one drive wants separate disconnects.

Resolution: 
Not recommended on Altivar drives.
The GV2 have a fixed frequency range 50 to 60hz.
Possible intermittent trips used with the drive's PWM output.
 
Was this helpful?
What can we do to improve the information ?