Technical FAQs

Ask a Question

What are the MTTF and MTBF data of Compact NSX circuit breakers?

MTTF is the average time until the first failure of the device occurs. The MTTF data of the Compact NSX circuit breakers is available in the attached file.

MTBF is the main time between failures. This parameter is calculated for products which are repaired after failure. The Compact NSX devices and its components are changed in case of a failure, not repaired. This is the reason why MTBF is not calculated for these devices.
Was this helpful?
What can we do to improve the information ?