Browse FAQs

Does the ATV212 drive support ethernet protocol?

Published date: 07 June 2019

Issue:
Does the ATV212 drive support ethernet protocol?

Product Line:
Altivar 212

Environment:
All

Cause:
Communications.

Resolution:
No, the ATV212 drive does not have ethernet communications available.  It supports Modbus RTU, Metasys N2, BACnet, and LonWorks protocols.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.