Technical FAQs

Ask a Question

What would cause an enclosed E-flex or MCC drive to continue to run from the network even when the HOA is in the off position?

Issue:
What would cause an enclosed E-flex or MCC drive to continue to run from the network even when the HOA is in the off position?

Product Line:
E-flex, M-flex, MCC

Environment:
All 

Cause:
Force to local is not on or the command switch of off does not match the hand function.

Resolution:
Check the status of the logic input used for hand off auto normally LI3.   The logic for Off and Hand should be ON or 1 and auto needs to be off or 0.   Be aware that Auto (Net control) mode and OFF mode can not be the same logic.  This means when you are OFF he drive can still run from the NET control. 
Was this helpful?
What can we do to improve the information ?