Technical FAQs

Ask a Question

ATV71 using Ethernet IP, How can I read when the drive is accelerating or decelerating?

Issue:   ATV71 using Ethernet IP, How can I read when the drive is accelerating or decelerating?
 
Product Line:   ATV71
 
Environment:  ALl using Ethernet IP
 
Cause:   Reading when drive is in ACC or DEC
 
Resolution:   Register 3253 bit 13 is ACC in progress, Bit 14 is Dec in progress.
 
Was this helpful?
What can we do to improve the information ?