Technical FAQs

Ask a Question

How to clear the BMxCRA312x0 adapter's Stored IP address



 To clear the BMxCRA312x0 adapter Stored IP address. 

 Power down the BMxCRA312x0 adapter. 
 Set right rotary switch to 'Clear IP' position. Set left rotary switch to zero position. 
 Power on the BMXCRA31210 adapter. 
 After 5 seconds, power down the BMxCRA312x0 adapter. 
Set right rotary switch to '1' position. Set left rotary switch to zero position. 
Power on the BMxCRA312x0 adapter and it should connect via DHCP. 


 
Was this helpful?
What can we do to improve the information ?