Technical FAQs

Ask a Question

What is the total available milliamps on the 24VDC supply in the ATV930 drive?

Issue:   What is the total available milliamps on the 24VDC supply in the ATV930 drive?
 
Product Line:   ATV930 Process drive
 
Environment:  All
 
Cause:   Internal 24VDC available ma
 
Resolution:   per the ATV930 install manual:  Current: maximum 200 mA for both 24 Vdc terminals
 
Was this helpful?
What can we do to improve the information ?