Technical FAQs

Ask a Question

What is the total available milliamps on the 24VDC supply in the ATV630 drive?

Issue:   What is the total available milliamps on the 24VDC supply in the ATV630 drive?
 
Product Line:   ATV630  Process
 
Environment:  All
 
Cause:   24VDC supply ma
 
Resolution:   Per the ATV600 install manual:   Current: maximum 200 mA for both 24 Vdc terminals
 
Was this helpful?
What can we do to improve the information ?