Technical FAQs

Ask a Question

Where can I find pinout information on the ATV58 modbus connection DB9 connector?

Issue:
Where can I find information on the ATV58 modbus connection DB9 connector?

Product Line:
Altivar ATV58

Environment:
All 

Cause:
Modbus

Resolution:
ATV58 modbus wiring  
Pins
7=D(B) (1) +
3=D(A) (0) -
4= 0V or com

 
Was this helpful?
What can we do to improve the information ?