Technical FAQs

Ask a Question

What would cause the assembly 106 and 107 I/0 tables in somove to reset to default after closing out somove and or power cycling the ATV930 drive?

Issue:
What would cause the assembly 106 and 107 I/0 tables in somove to reset to default after closing out somove and or power cycling the ATV930 drive?

Product Line:
Somove and ATV930 

Environment:
All 

Cause:
assemblies 106 and 107 are not supported

Resolution:
Assemblies 106 and 107 are only supported in Somove and not the Drive so the drive will not retain the settings and will reset back to default after power cycle or if you open up somove again and copy from drive to PC. 
Was this helpful?
What can we do to improve the information ?