Technical FAQs

Ask a Question

How do I program an ATV630 drive to toggle between HMI and Remote controls?

issue:
How do I program an ATV630 drive to toggle between HMI and Remote controls?

Product Line:
ATV630   ATV930 

Environment
All serial numbers

Cause:
Dual controls 

Resolution:

Enable the Local/Remote button:
Complete Settings >  Command and Reference > HMI cmd  set to bumpless.

Press the Local/Remote button to toggle between HMI and remote control. 
Was this helpful?
What can we do to improve the information ?