Technical FAQs

Ask a Question

Osisense XC - Contact diagram of the limit switch ZCMD37L*+ZCE63 or ZCMD37L*+ZCE62

Find hereafter the contact diagram of the limit switch ZCMD37L*+ZCE63 or ZCMD37L*+ZCE62. It is not shown into the Osisense XC standard catalogue.

Was this helpful?
What can we do to improve the information ?