Browse FAQs

What is the closing plate part number for the rectangular HOA selector switch on a 8538 and 8539 Combo starters with NEMA 1 enclosures Size 0 - 4?

Published date: 26 July 2019

Issue:
Closing plate part number for the rectangular HOA selector switch on a 8538 and 8539 NEMA 1 starters Size 0 - 4?

Product Line: 
Nema combonation starters

Environment:
8538 8539

Cause:
Needs the closing plate part number for the rectangular HOA selector switch on a 8538 and 8539 Combo starters with NEMA 1 enclosures Size 0 - 4.

Resolution:
9999SG1


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.