Technical FAQs

Ask a Question

If you program multiple relays R1 or R2 to CTA or current threshold attained will you get two separate threshold values for each relay?

Issue:
If you program multiple relays R1 or R2 to CTA or current threshold attained will you get two separate threshold values for each relay?

Product Line:
ATV61, ATV71 ATV630 and ATV930 

Environment:
All 

Cause:
All 

Resolution:
You can program multiple relays to the current threshold attained however there is only one setting for the CTD current threshold reached low and high setting. 
 
Was this helpful?
What can we do to improve the information ?