Browse FAQs

How do I read my motor power on an ATV61 drive over bacnet?

Published date: 14 May 2019

Issue:
How do I read my motor power on an ATV61 drive over bacnet?

Product Line:
ATV61 series drives.

Environment:
All models and serial numbers equipped with Bacnet card, Either VW3A3315 or VW3A3319.

Cause:
ATV61 with Bacnet network.  Need to read motor power

Resolution:
The Motor Power can be read on AVO#6, and is given as a percentage of the power rating of the drive itself.  For example, an ATV61HD75N4 is rated for 75KW, if AVO#6 reads 50%, this would indicate a motor power of 37.5%.  Other examples to decode the power rating of the ATV61 drives are below:
O75 = .75KW or 1HP.
U75 = 7.5KW or 10HP
D75 = 75KW or 100HP
*C63 = 630KW or 900HP.

*C75 version does not exist, ATV61HC63N4 is the highest.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.