Technical FAQs

Ask a Question

ATV630 What is the recommended corrective action when the motor runs in reverse with a run forward command?

Issue:
ATV630 What is the recommended corrective action when the motor runs in reverse with a run forward command?

Product Line:
Altivar 630 Process Drives

Environment:
All

Cause:
The phase rotation is inverted coming out of the drive going to the motor

Resolution:
To correct the motor rotation swap two motor leads on the drive output terminals (T1,T2,T3)



 
Was this helpful?
What can we do to improve the information ?