Browse FAQs

What is the maximum number of IP address allowed for Port Security with a Connexium Managed Switch ?

Published date: 26 February 2019

Title
Port Security with a Connexium Managed Switch
 
Issue
Port Security with a Connexium Managed Switch
 
Product Line
Connexium
 
Environment
Connexium
 
Cause
N/A
 
Resolution
 The manual does specify that each port on the Connexium switch can be set to only recognize a maximum of 10 IP addresses. 
The entered allowed IP source address for a port has to use the format: nnn.nnn.nnn.nnn (nnn: decimal number 0..255). 
For example: port-sec allowed-ip <IP Address 1> <IP Address 2> ... <IP Address 10>

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.