Technical FAQs

Ask a Question

Why project file converted "in the form of .DWG" fails sometimes in Ecodial Advance calculation?

The Ecodial Advance Calculation files can be saved in the form ".DWG", but the tool is not supporting all the components of Ecodial. This limitation is known for many versions of Ecodial. Overall this DWG conversion services, Ecodial needs to be improved.
Workaround:
1. Save the project in the local computer in the DXF format.
2. Open the locally saved DXF file in the AutoCAD.
3. Now click on the "Save as" and save the file in the DWG format which should work fine.
Was this helpful?
What can we do to improve the information ?