Browse FAQs

Is there a parameter change history on an Altivar 31?

Published date: 27 February 2019

Issue:
Can we csee what parameters were changed and what were not on an Altivar 31?

Product Line:
Altivar 31, ATV31

Environment:
All

Cause:
NA

Resolution:
No, there is no change history available on the drive.  If you connect using Somove, you can see the Modified parameters.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.